This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Figure (a) shows an example of an IGBT application circuit. Surge voltage is generated when the IGBT turns off while it is carrying the load current. Surge voltage is caused by a sharp change in IGBT current (-diC/dt) as well as the package and wire stray inductance (LS). At this time, VCEP = LS・diC/dt+VCC is applied to the IGBT instantaneously. The IGBT is permanently damaged if a voltage exceeding its breakdown voltage is applied. A primary solution for this is to reduce the stray inductance (LS) of the main current path. It is therefore necessary to increase the width and reduce the length of the wires. If it is difficult to reduce stray inductance, the switching speed of the IGBT should be reduced by increasing the value of an external gate resistor connected in series with the gate. Care should be exercised, however, because this causes its switching loss to increase. Surge voltage can also be reduced by inserting a snubber circuit between the collector and emitter terminals of the IGBT. However, the snubber circuit causes charge/discharge loss, increasing overall circuit loss.