This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
The overcurrent protection function of the eFuse ICs is a function that clamps (holds) the output current to prevent it from exceeding the overcurrent limit (ILIMIT) when the output current increases because of abnormal loads or short-circuiting, thereby preventing instantaneous power-off and protecting the devices from degradation or breakdown due to heat generation. Toshiba eFuse ICs can be set optimally by the variable overcurrent protecting function using external resistors. Robust protection can be realized by the double overcurrent protection function in addition to the short-circuit protection function that turns on when the output current greatly exceeds the limit current in an extremely short time.
Our eFuse IC TCKE8 series have an overcurrent clamping function with high accuracy from low temperature to high temperature with respect to the overcurrent limit. The normal overcurrent protection function (circuit break) stops the output current immediately when the overcurrent limit is reached, and the output voltage drops. On the other hand, the eFuse IC clamps the current and keeps it from flowing more than the set current. By keeping the output voltage within the breakdown voltage of the post-stage IC, more stable power supply can be constructed.
Stock Check & Purchase
require 3 characters or more.