Contact us

A new window will open A new window will open

Electrical characteristics of MOSFETs (Dynamic Characteristics tr/ton/tf/toff)

Switching characteristics
Since power MOSFETs are majority-carrier devices, they are faster and capable of switching at higher frequencies than bipolar transistors.
Switching time measurement circuit and input / output waveform are shown below.



  1. td (on): Turn-on delay time
    The time from when the gate-source voltage rises above 10% of VGS until the drain-source voltage reaches 90% of VDS
  2. tr:Rise time
    The time taken for the drain-source voltage to fall from 90% to 10% of VDS
  3. ton:Turn-on time
    The turn-on time is equal to td (on)+ tr.
  4. td (off):Turn-off delay time
    The time from when the gate-source voltage drops below 90% of VGS until the drain-source voltage reaches 10% of VDS
  5. tf:Fall time
    The time taken for the drain-source voltage to rise from 10% to 90% of VDS
  6. toff:Turn-off time
    The turn-off time is equal to td(off)+ tf.


Data sheet description

Characteristics Symbol Min Typ Max Unit
Switching time Rise time tr 13 ns
Turn-on time ton 26
Fall time tf 14
Turn-off time toff 63
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.