Contact us

A new window will open A new window will open

How do N-channel MOSFETs work?

In the planar MOSFET shown below:

  1. Apply voltage between drain and source in positive polarity. (Drain-source voltage: VDS)
  2. Apply voltage between gate and source in positive polarity. (Gate-source voltage: VGS)
  3. As a result, electrons are attracted to P layer under a gate insulator film and P layer becomes N layer. (Such P layer that becomes N layer is called an “inversion layer.”)
  4. All regions of MOSFET become N layer (from drain side: “N+”-”N-”-”inversion layer(N)”– “N+”) due to inversion mentioned in 3.
  5. As a result, MOSFET works as a resistor, and drain current determined by applied VDS and load flows.

Structure and operation of planar MOSFET

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.