This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
It is an intrinsic semiconductor doped with boron (B), indium (In), etc. Where silicon and boron are bonded, lack of an electron can be brought about by adding a small amount of boron to pure silicon. This lack is called a hole. When voltage is applied in this situation, an adjacent electron moves to this hole and the place the electron is removed from becomes a new hole. Holes move to "–" electrode in sequence.