This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
As smartphones, tablets, point-of-sale (POS) terminals, and other mobile devices become ever more prevalent, they are becoming increasingly exposed to electrostatic discharge (ESD) from a charged human body or object, making them more vulnerable to permanent damage or deterioration. There are two types of ESD strikes: 1) contact discharge caused by contact with an exposed connector and 2) air discharge that produces an electric spark, invading an antenna or internal loop wiring. It is necessary to protect mobile devices from these ESD events. Nowadays, it has become the norm to test the ESD tolerance of exposed leads and add ESD protection as necessary.
Therefore, these circuits are sometimes not protected against ESD. An antenna is connected to radio-frequency (RF) ICs and other sensitive devices. Although the RF IC shown in Figure 1 incorporates ESD protection circuits, they typically provide an ESD tolerance of less than 1 kV HBM (human body model). Although this ESD protection level is sufficient in manufacturing and other ESD-controlled environments, it does not suffice for environments in which mobile devices are generally used. Proper ESD protection must be considered not only for the ESD protection diode alone, but also for the entire system, including the ESD protection circuitry incorporated in the RF IC.
This application note provides an answer to one of the frequently asked questions about the considerations required for the selection of ESD protection diodes.
ESD enters an electronic system from an antenna and might damage or degrade an RF circuit. In particular, RF front-end ICs such as global positioning system (GPS) receivers are fabricated using a nanoscale process in order to satisfy system requirements. ICs with smaller geometries are less tolerant of ESD.
Receive-only antenna systems for GPS and FM radios generally handle micro-power signals whereas Wi-Fi® and other transceiver antennas transmit high-power signals in transmit mode. However, the requirements for ESD tolerance and high-power signal transmission are contradictory. The following sections describe the considerations for the ESD protection of RF transceiver antenna lines from three perspectives:
* Wi-Fi is a registered trademark of Wi-Fi Alliance.
* Other company names, product names, and service names may be trademarks of their respective companies.