This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
The short-circuit protection function prevents overcurrent by switching off the output of the eFuse IC in the event of a short circuit caused by an abnormality in the power supply line or load.
Short-circuit protection is a protective function, also known as fast trip.
The following is an explanation based on the operation example of the TCKE8 series.
Please check each of the data sheets for details.
When a large current (exceeding the set current) flows instantaneously through the MOSFET, the eFuse IC determines that the output is short-circuited, and shuts down the MOSFET in a very short time. After shutdown, the MOSFET is automatically turned on by a timer set inside the eFuse IC. At this time, if there is no abnormality in the subsequent ICs or circuits, eFuse IC operates normally. However, if there is a reason for overcurrent to flow, eFuse IC performs overcurrent protective operation.
In the overcurrent protection the of auto-retry type, the output current is limited by overcurrent protection, the output is shut down when the junction temperature rises to the temperature of thermal shutdown, and when the junction temperature drops, the output turns on again to limit the output current.
After that, the recovery cycle is repeated by the following cycles until the overcurrent is eliminated.
The overcurrent protection of the latch type shuts down the output when an overcurrent is detected and retains the output off state. Releasing the output-off is performed by once dropping EN/ UVLO signal to the "L" level and then inputting the "H" level signal again.
Please refer to the following pages and documents for product lineup and other documents.
* Company names, product names, and service names used in this FAQ may be of their respective companies.