This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
In the event of an overcurrent condition, our LDO regulators are protected by foldback.
The term “foldback” is derived from the shape of the output current (IOUT)-vs-output voltage (VOUT) curve that folds back as shown in Figure 1 during protection operation.
Under a short-circuited load condition, foldback reduces IOUT as VOUT decreases. When VOUT has dropped to zero, it keeps the output current at a limited constant level.
When the overcurrent condition has disappeared, VOUT returns to the normal level automatically.
If an output capacitor or a capacitive load is connected to the output pin, VOUT increases while IOUT is limited by foldback.
The following documents also contain related information.