This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
The step-down DCDC converter and LDO regulator both have a voltage-down function.
DCDC converter and LDO regulator are compared below.
| LDO | DCDC converter | |
|---|---|---|
| Number of peripheral parts |
✔✔✔ | ✔ |
| Stand-by power consumption |
✔✔✔ | ✔ |
| Noise characteristics |
✔✔✔ | ✔ |
| Power efficiency |
✔ | ✔✔✔✔ |
✔:Average ✔✔:Good、 ✔✔✔:Very Good ✔✔✔✔:Excellent
DCDC converters are often selected in the following situations:
In the following cases, LDO are often selected.
The main advantages of LDO are described below.
Advantage of LDO 1: Simple circuitry with fewer components
LDO has a small circuitry and can be powered by external components. Therefore, it is cheaper and consumes less current. In addition, since the control is also simple, voltage can be output without fine adjustment.
Benefits of LDO 2: Low-noise power output
Since LDO controls the voltage by the movement of the variable resistor, the voltage can be outputted with relatively low noises.
DCDC is switched and smoothed by a LC filter, so it can be used in a steady state.
The power is waving. (voltage ripple)
The following documents also contain related information.