This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Op amps are very high gain devices. To achieve stable operation, op-amps are used with negative feedback. The gain of the device alone is called open loop gain, and the gain when configuring a negative feedback circuit is called closed loop gain. Closed-loop gain is not device-specific and is usually determined by the feedback network.
Above the cutoff frequency where the gain drops -3dB below the passband, the open-loop gain halves when frequency doubles. (On a logarithmic scale, it has a slope of -6 dB/oct or -20 dB/dec.) .
The closed-loop gain (Gv) of the negative feedback circuit shown in Fig. 2 is calculated as -R2/R1.
The following documents also contain related information: