This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
If the input signal trace of a CMOS logic IC is in the vicinity of an output signal trace of another IC, crosstalk noise might be generated. Check if another trace is in the vicinity of the input signal trace or runs adjacently in parallel.
Generally, the following countermeasures can be considered:
For a description of crosstalk, please refer to “Precaution when Designing Circuits: Logic ICs”.
CMOS Logic ICs Usage Considerations (PDF:1.61MB)
The following documents also contain related information.