This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
The unused output pins of general-purpose logic IC must be open.
However, for pins that may become inputs (such as bus pins) like bi-directional bus buffers such as 245, please connect both ends of the input and output to the power supply or GND via pull-up/pull-down resistors. To avoid unnecessary current flow, it is recommended to pull up or pull down both ends of the bi-directional bus buffer to the same potential.
The following documents also contain related information.