This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
To supply a stable voltage with minimal noise from the power supply to the IC, it is recommended to put a decoupling capacitor between GND and the power supply.
There are two types of decoupling capacitors: ceramic capacitors, which filter high-frequency noise, and electrolytic capacitors, which filter low-frequency noise. The ceramic capacitor should be placed close to the IC (refer to the figure below). Placing it at a distance from the IC not only reduces the effectiveness of filtering high-frequency noise due to the impedance of the wiring but may also cause the IC’s switching noise to be radiated. The capacitance value of the capacitor varies depending on the product, therefore, please refer to the application note of the product.
By adding a decoupling capacitor, a stable voltage with minimal noise can be supplied from the power supply to IC.
The following documents also contain related information.