This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
*This function runs on Twin Builder™ and requires Twin Builder™ to operate.
Step(1). Select steering scenario for steering. Currently, only Scenario A is preset.
Step(2). Press "Edit" to start WAVE VIEWER. Edit the steer scenario waveform as needed.
Step(3). Selects the motor control method. Two types of control methods are currently preset.
Step(4). Set various parameters of the motor.
J: Moment of inertia ψ: Chain magnetic flux
Ld: d-axis inductance p: Number of contacts
Lq: q-axis inductance Rs: Winding resistance
Step(5). Set the thermal resistance and heat capacity of the printed circuit board and heat sink. To configure a multi-stage RC circuit, input multiple resistance and capacitance values by separating them with a space.
Step(6). Set the simulation time.
Step(7). Selects the power semiconductor (MOSFET) used for 3-phase inverter circuitry. Double-click to jump to the product page.
Step(8). Run : Starts the simulation.
Setup Only : Saves the settings. No simulation is performed.
Option: The Advanced Settings window opens. Normally, this setting is not required. Refer to the following for details.
<Description of the detailed setting screen>
Accu-ROM™ is simulated under the following 4Step. Here you can make detailed settings for each Step.
1. Check Simulation :
Simulation for initial operation check.
2. Power Loss Control:
Simulation for reduced-order modeling of MOSFET model.
3. PreSim Control:
Simulation for reduced-order modeling of mechanical plant model. Operating Time of the main setting window is applied to End Time.
4. MainSim Control:
Simulation for reduced-order modeling of MOSFET and mechanical plant model. Operating Time of the main setting window is applied to End Time.
*Ansys® and all other ANSYS, Inc. product names are trademarks or registered trademarks of ANSYS, Inc. or its subsidiaries in the United States or other countries.
*Accu-ROM™ is a trademark of TOSHIBA CORPORATION Device & Storage Corporation.
*Other company names, product names, service names, and the like may be used by each company as trademarks.