* : Products list (parametric search)
* : Products list (parametric search)
* : Products list (parametric search)
* : Products list (parametric search)
* : Products list (parametric search)
* : Products list (parametric search)
* : Products list (parametric search)
* : Products list (parametric search)
* : Products list (parametric search)
Knowledge
This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Silicon carbide (SiC) is a wide-bandgap semiconductor with a bandgap of 3.26 eV, much higher than that of silicon (Si) (=1.12 eV). SiC provides high electric breakdown field and high thermal conductivity because of high atomic bond due to a low lattice constant (i.e., a short atom-to-atom distance).
Characteristics | Unit | Si | 4H-SiC |
---|---|---|---|
Bandgap | eV | 1.12 | 3.26 |
Electron mobility, μe | cm2/Vs | 1400 | 1000/1200 |
Hole mobility, μh | 600 | 120 | |
Electric breakdown field, Ec | V/cm | 3.0×105 | 2.8×106 |
Thermal conductivity, λ | W/cmK | 1.5 | 4.9 |
Saturation electron drift velocity, Vsat | cm/s |
1.0×107 | 2.2×107 |
Relative dielectric constant, ε | 11.8 | 9.7/10.2 |
When an SBD with a conventional structure is reverse-biased, the depletion region extends into the semiconductor as shown below. The area of the triangle formed by the electric breakdown field and the depletion region width represents the withstand voltage of an SBD. The depletion region depth is inversely proportional to the dopant concentration. Increasing the dopant concentration helps reduce the resistance of silicon and therefore the forward voltage (VF) of the SBD, but at the expense of withstand voltage (i.e., triangle area). The electric breakdown field of SiC is nearly 10 times that of silicon. As shown below, it is therefore possible to increase the withstand voltage (i.e., triangle area) of a SiC SBD relative to a Si SBD, even if it is heavily doped.
In addition, since the depletion layer is less stretched by the higher concentration, the thickness of the chip can be thinner than in the case of Si. The thickness of the semiconductor (Si or SiC) can be considered as series resistance in the forward direction, and so the forward voltage can be improved by reducing the thickness.
Stock Check & Purchase
require 3 characters or more.
Part Number | Authorized Distributor | Stock Quantity | Date | Shopping Cart |
---|