Knowledge
This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
The overcurrent protection function of the load switch IC is a function that protects the device from degradation or breakdown caused by heat generated by the device itself by suppressing the output current when the output VOUT terminal is in an unintended short-circuit mode. It is also called current limit or OCP (Over Current Protection). Toshiba load switch ICs employ a foldback-type protection circuit control method, which contributes to safety design.
We mass-produce a load switch IC with a built-in overcurrent protection function of the foldback type.
For example, when the output current reaches the internal overcurrent limit when the load is short-circuited, the MOSFET inside the load switch is turned off, thereby reducing the output voltage VOUT and limiting the output current IOUT. This function suppresses element heat generation during overcurrent operation. The overcurrent value has a fixed value for each product, and the product lineup covers a wide range from a low current value of several hundred mA to over 1.0 A.
Stock Check & Purchase
require 3 characters or more.