This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
This is the resistance between the drain-source when MOSFET is on at the specified gate-voltage.
To measure the drain-source resistance (RDS(ON)), first, apply a voltage that exceeds the specified threshold voltage (Vth) between the gate and source. Next, apply the specified current source (ID) and measure the voltage drop (VDS) between the drain and source.
Using these measurements, you can calculate the RDS(ON) for the specified gate-source voltage (VGS) using the formula: RDS(ON)=VDS/ID.
NOTE) Make sure that the open voltage of the constant-current power supply is equal to or less than the withstand voltage between the drain and the ground.
Please also refer to the following page.