Contact us

A new window will open A new window will open

Is it OK to use the body diode (parasitic diode) between the drain and source for a particular purpose?

Yes, you can. Actually this diode is actively used in motor drive circuits, power supply circuits, etc. In the MOSFETs used for these applications, the body diode specification is described in the data sheet.

(The specified characteristics differ from product to product. Ta=25℃ unless otherwise specified.)

Characteristic Symbol Unit Description
Reverse drain current(DC)
Reverse drain current(pulsed)
IDR
IDRP
A The maximum current that can flow to the body diode of a MOSFET in the forward direction
Diode forward voltage VDSF V Drain-source voltage that appears when a current is applied to the body diode of a MOSFET in the forward direction
Reverse recovery time trr ns The time trr and the amount of charge Qrr required for the reverse recovery current to reach zero during the reverse recovery operation of the body diode under the specified test conditions. The peak current during this period is Irr.
Diode reverse recovery charge Qrr μC
Diode peak reverse recovery current Irr A
Diode dv/dt capability dv/dt V/ns The maximum voltage ramp allowed during the reverse recovery time of the diode

Data sheet description

Characteristic Symbol Test Conditions Min Typ Max Unit
Diode forward voltage VDSF IDR = 30.8 A, VGS = 0 V - - -1.7 V
Reverse recovery time trr IDR = 15.4 A, VGS = 0 V
-dIDR/dt = 100 A/μs
- 135 220 ns
Diode reverse recovery charge Qrr - 0.6 - μC
Diode peak reverse recovery current Irr - 10 - A
Diode dv/dt capability dv/dt IDR = 15.4 A, VGS = 0 V, VDD = 400 V 50 - - V/ns

For use of this diode, the maximum channel temperature (Tch (max)) specification is also applicable.

Electrical Characteristics: Power MOSFET Application Notes (PDF:1,092KB)
https://toshiba.semicon-storage.com/info/docget.jsp?did=13415

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.