This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Here is the operation sequence of brushed DC motor.
・At the base point, coil 1 is situated at the S pole and coils 2 and 3 at the N poles, and they rotate clockwise by the attraction and the repulsion.
・At the position rotated 30 degrees to the right, coil 1 is situated at the S pole and coil 2 remains the N pole. The current stops flowing in coil 3, and then continues to rotate right by the attraction and the repulsion.
・At the position rotated 60 degrees to the right, coil 1 is situated at the S pole, coil 2 remains the N pole, and coil 3 is situated at the S pole, and then continues to rotate right by the attraction and the repulsion.
・At the position rotated 90 degrees to the right, no current will flow in coil 1. Coil 2 is situated at the N pole, and coil 3 remains the S pole, and then continues to rotate right by the attraction and the repulsion.
At the 120-degree position, coil 3 rotates to coil 1 position that is the base point, coil 1 to coil 2 position that is the base point, and coil 2 to coil 3 position that is the base point.