2-4. Sequence of a Brushless Motor

Sequence of a Brushless Motor

Here is the operation sequence of brushless motor. (in case of square-wave drive)
・At the base point, the V phase becomes the S pole and the W phase becomes the N pole, and it rotates clockwise by the attraction and the repulsion.
・The current flowing to the coil is switched every 60 degrees, and the S pole/N pole of each phase is switched every 120 degrees.

Chapter 2 Driving Principle of a Brushless Motor

2-1-1. Driving Principle of a Motor (1)
2-1-2. Driving Principle of a Motor (2)
2-2. Brushed DC Motors and Brushless Motors
2-3. Sequence of a Brushed DC Motor
2-5. Relation Between a Pole, a Phase, and a Slot
A new window will open