This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
The step angle is the basis of the movement of a stepping motor.
The step angle depends on the total number of magnetic poles of the motor.
The step angle is determined by the formula:
Step angle = 360 degrees / N where N = (NPH x PH)
The motor types are usually referenced as “PH-phase / N-pole motor” (e.g. 2-phase / 4-pole on the left side and 3-phase / 6-pole on the right side)
For example, in case of a 2-phase 4-pole motor, the step angle will be 90 degrees.
The stepping motor is rotated as a result of performing each step operation continuously.