This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
As an example, the figure (Definitions of Electrical Characteristics) contained in the datasheet of a unidirectional TVS diode are given below. Although a TVS diode has many voltage and current specifications, attention should be paid to the working peak reverse voltage (VRWM) here.
VRWM is a threshold below which the TVS diode remains off when Ta=25°C. It is necessary to select TVS diodes with a VRWM higher than the maximum voltage of the signal lines to be protected.
However, TVS diodes with an excessively high VRWM (i.e., high clamp voltage) cause more energy to flow into the device under protection in the event of ESD. Select the optimum TVS diodes according to the design specifications.