This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Some bus switches have a tolerant function, while others do not. Table 1 lists whether each series of bus switches has a tolerant function or not, so please refer to it. However, for details, please check the data sheet of the device you are using. If there is a possibility that a signal may be input to the I/O terminal of the bus switch when the power is turned off, select a product with a tolerant function.
| Category | Switch Configuration |
VCC (V) | Type | Product Series | Tolerant Function | ||
|---|---|---|---|---|---|---|---|
| Control Pin | Switch I/O | ||||||
| Low Voltage | SPST | 1.65~3.6 | N-ch+P-ch | ✔ | ✔ | ||
| SPDT | TC7MBL Series | ✔ | ✔ | ||||
| SP4T | TC7MBL Series | ✔ | ✔ | ||||
| 5 V | SPDT | 1.65~5.5 | ✔ | - | |||
| SPDT | TC7SB Series | ✔ | - | ||||
| Dual Supply level shifting |
SPST | VCCA 1.65~5.0 |
VCCB 2.3~5.5 |
N-ch | ✔ | ✔ | |
| SPDT | TC7MPB Series | ✔ | ✔ | ||||
The tolerant function of the input/output terminals (I/O terminals) of the bus switch
As for how to check the tolerant function of the bus switch, please check the rating of the "switch input/output voltage" item in the operating ranges of the data sheet. Table 2 shows the operating range of TC7MBL3257CFT as an example of a device with a tolerant function. When VCC = 0 V or switch = OFF, the switch input/output voltage (VS) does not depend on the power supply voltage and can input signals within the range of the power supply voltage. Therefore, even if a signal is input when the power is off, the device will not be damaged.
Table-2 TC7MBL3257CFT operating ranges
And Table-3 lists the operating ranges of TC7WB66CFK as an example of a device that does not have a tolerant function. When VCC = 0 V or the switch is OFF, the switch input/output voltage (VS) is 0 to VCC, so the input signal depends on the input voltage. In other words, the input signal cannot be input when the power is cut off.
Table-3 TC7WB66CFK operating ranges
The following documents also contain related information.