This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
The area where transistors and MOSFETs are not destroyed or prone to deterioration is called the safe operating area (SOA). It is important that the operating point is within this curve. In the case of a bipolar transistor, the curve in the SOA is divided into a thermal dissipation limit and the limit given by secondary breakdown. In the case of a MOSFET, the SOA is divided into a current limit, a thermal dissipation limit, a limit given by secondary breakdown, and a voltage limit. Recently, there are products for which an on-resistance limit area is specified in the data sheet.
Maximum Ratings: Power MOSFET Application Notes (PDF:1,075KB)