This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
As shown in Fig. 1, Toshiba’s DTMOS series applies Superjunction (SJ) structure in which P and N layers are alternately arranged in the drift layer. The high accurate SPICE model (G2 model) for SJ structure MOSFET (SJ-MOSFET) developed by Toshiba can express the saturation characteristics in the high current region of Drain current vs Drain-source Voltage (ID-VDS) charactaristics. And the abrupt capacitance change depending on the MOSFET Drain voltage shown in Fig. 2 is also reproduced by using the arbitrary function.
Fig. 3 shows the reproduction level (called "fitting accuracy") by comparing the actual measurement of ID-VGS characteristics and ID-VDS characteristics of our SJ-MOSFET product TK040N65Z with the simulation using our SPICE model. In the High voltage breakdown MOSFET such as SJ-MOSFET, Drain Current (ID) saturate due to the resistance effected by the deep and long drift layer. In our SPICE model, this saturation characteristic is expressed by a non-linear resister (RX) which applied to the drain side so the simulation curve can show actual measurement with accuracy even in the high current region.
Fig. 4 shows a comparison between actual measurement and simulation of the VDS dependencies on the Input capacitance (Ciss), the Output capacitance (Coss), and the Reverse transfer capacitance (Crss). The capacitance characteristics of SJ-MOSFET change rapidly with the depletion layer extending from the PN-junction due to the SJ structure. On the other hand, Toshiba's SPICE model can show the non-linearity of the measurement values with high accuracy by additional arbitrary functions of non-linear capacitance combination of Gate-souece (Cgs), Gate-drain (Cgd) and Drain-source (Cds).
Fig. 5 shows a inductive load switching circuit diagram using SJ-MOSFET product TK040N65Z. And Fig. 6 shows the comparison between the actual waveform and the simulation using the G2 model for SJ-MOSFET as described above. By using our G2 model which can express the non-linearity of the capacitance characteristic with high accuracy, we can see very accurate waveforms that the rising of VDS and oscillation of VDS and ID, associated with oscillation of dVDS/dt or VGS. Our G2 model for SJ-MOSFET is a SPICE model that can sufficiently verify dynamic properties such as switching operation.
Fig. 6: Comparison of actual measurement and simulation of turn-off waveforms in inductance load switching circuit
(a)VGS (b)VDS (c)ID
Our high accurate SPICE model (G2 model) can reproduce the actual switching waveforms with high accuracy. The circuit verification by using high-accuracy simulation in advance of the actual production may reduce the double work for the circuit modification and help the development time shorten. Toshiba's high accurate SPICE model (G2 model) supports your circuit development and analysis effectively.