This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Currently, this has been released to the public for some of our low voltage MOSFET, mid to high voltage MOSFET and in-vehicle MOSFET products, but we plan to successively expand this range to other products, including SiC MOSFET products. Please use G0 model to check the operation without spending a long time, and use the G2 model to know characteristics accurately. Please be sure to try the G2 model as it will be effective for more accurate simulations such as loss characteristics.
G0 and G2 models can be downloaded from above linkage destination. If you select the desired model and click here, the zip file with the following name will be downloaded.
For PSpice model: (product name)_PSpice_(registration date).zip
For LTspice models: (product name)_LTspice_(registration date).zip
If you unpack it, you will find a total of four files in the unpacking folder: library files and symbol files for G0 and G2 model each.
(for PSpice)
(Product name)_G0_00_PSpice_revX.lib G0 model library file for PSpice
(Product name)_G0_00_PSPICE_REVX.OLB G0 model symbol file for PSpice
(Product name)_G2_00_PSpice_revX_enc.lib G2 model library file for PSpice
(Product name)_G2_00_PSPICE_REVX_ENC.OLB G2 model symbol file for PSpice
(for LTspice)
(Product name)_G0_00_LTspice_revX_enc.lib G0 model library file for LTspice
(Product name)_G0_00_LTspice_revX_enc.asy G0 model symbol file for LTspice
(Product name)_G2_00_LTspice_revX_enc.lib G2 model library file for LTspice
(Product name)_G2_00_LTspice_revX_enc.asy G2 model symbol file for LTspice
RevX are revision numbers, rev1, rev2, etc.
Use the G0 library and symbols for the G0 model and the G2 library and symbols for the G2 model.
* PSpice® is a registered trademark of Cadence Design Systems, Inc.
* LTspice® is simulation software and registered trademarks of Analog Devices, Inc.
* Cadence, the Cadence logo, OrCAD and OrCAD logo are trademarks or registered trademarks of Cadence Design Systems, Inc.
* Other company names, product names, and service names may be trademarks of their respective companies.