This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
DSOP Advance has a metallic plate (E-Pad) on the top of the packaging to dissipate heat from the chips. Improved heat dissipation through this metallic plate reduces the increase in MOSFET temperatures during high-current conduction and contributes to improved power density and efficiency of power supply circuits. Thermal resistivity Rth(ch-c) of DSOP Advance is reduced by 45% compared with SOP Advance of the same package size. Since the DSOP Advance footprint patterns are the same as those of the conventional SOP Advance, they can be replaced without changing the layout of the printed circuit board.
Replacing Toshiba's 30V MOSFET TPHR9003NL with the TPWR8503NL reduces MOSFET temperatures by 10.3°C. When a heat sink is mounted, the device temperature is reduced by 26℃ at the maximum.
The figure below shows the results of comparing heat dissipation simulations of SOP Advance and DSOP Advance. The upper part is a side view of the heat dissipation condition, and the lower part is its top view. Double-sided heat dissipation type DSOP Advance reduces MOSFET temperatures by approximately 40% compared with single-sided heat dissipation type SOP Advance.
Switched Mode Power Supply Library is the service which can select and download various basic topologies of power supply unit based on your actual requirement to verify the behavior of MOSFET with your simulation environment.
A MOSFET selection tool that allows circuit and thermal simulation on the Web.
Stock Check & Purchase
require 3 characters or more.