This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Whereas rectifier diodes are used in sub-500 Hz applications, FRDs are used in several kHz to 100 kHz switching.
Fast Recovery Diodes (FRDs) have the same withstand voltage as rectifier diodes, short reverse recovery time (trr), and low reverse recovery current. Loss due to recovery current is called switching loss. Since this recovery current and reverse recovery time are almost constant, the higher the frequency, the higher the ratio of switching loss to the total loss.
It is used in applications from several kHz to 100 kHz at voltages at which Si Schottky barrier diodes (Si-SBDs) cannot be used (reverse bias applied to the diode is several tens of V or more).
It is suitable for use in switching power supplies, inverters and DC-DC converters.
For products, please refer to the following links.