What is avalanche in MOSFET? (avalanche capability)

When a MOSFET is turned off, an avalanche breakdown occurs if the voltage applied between the drain and source exceeds the absolute maximum rating VDSS. Even if the DC voltage of the drain is within the rating, a surge voltage may be superimposed on this DC voltage due to factors such as stray inductance in the wiring, causing it to exceed the maximum rating. During an avalanche breakdown, a current flows suddenly, which may lead to avalanche destruction. When designing a circuit, you should select a MOSFET with a drain-source voltage VDSS that has a sufficient margin for the maximum drain voltage, even though there are products with guaranteed avalanche capability. Also, take the measures described below to prevent surge voltages from occurring.

Fig. 1 Switching circuit and surge voltage and current waveforms at turn-off:This is a waveform diagram showing how a surge voltage occurs between the drain and source due to the effect of parasitic inductance when a MOSFET is turned off.
Fig. 1 Switching circuit and surge voltage and current waveforms at turn-off

Avalanche breakdown of MOSFET
During the transitional timing when a MOSFET goes from on to off, a surge voltage may be applied between the drain and source due to the influence of parasitic inductance in the circuit. (See Fig. 1)
When this surge voltage is applied as a reverse bias to the MOSFET , free electrons in the pn junction of the internal parasitic diode (refer to Fig. 2 the equivalent circuit) are accelerated and gain high kinetic energy.
These high-energy electrons collide with atoms, releasing additional free electrons and generating electron-hole pairs. The newly generated electrons are also accelerated by the high electric field, creating more electron-hole pairs in a chain reaction. As a result, the current rapidly increases, and a large current—known as avalanche current (IAS)—flows. This phenomenon is called avalanche breakdown.
For more information on avalanche breakdown, please refer to section 2.4 "Zener Diodes" in the referenced document.
Application Note: Basics of Diodes (Types and Overview of Diodes) (1.8MB)

Fig. 2 MOSFET equivalent circuit: Avalanche breakdown occurs due to the parasitic diode, and the avalanche current activates the parasitic bipolar transistor, creating a short circuit.
Fig. 2 MOSFET equivalent circuit
Fig. 4 Avalanche measurement circuit,   voltage and current waveforms: Avalanche measurement circuit and current and voltage waveforms when avalanche breakdown occurs.
Fig. 4 Avalanche measurement circuit ,voltage and current waveforms

About Avalanche Breakdown
Avalanche breakdown can be classified into two main types: thermal breakdown and current-induced breakdown caused by a parasitic transistor.
1. Thermal Breakdown
Fig. 4 shows an avalanche test circuit and its waveform. In this circuit, when the MOSFET turns off, the inductance L attempts to maintain the current that was previously flowing. As a result, a reverse voltage is generated by the inductance, and if the drain-source voltage exceeds the rated VDSS​, avalanche breakdown may occur.
During this breakdown period, avalanche current (IAS) flows through the MOSFET. The device experiences power loss due to the combination of this avalanche current and the breakdown voltage BVDSS​. This power loss causes the junction temperature Tj​ of the device to rise, potentially leading to device failure. This energy loss is referred to as avalanche energy (EAS) and is an important parameter in circuit design.

Fig. 3 MOSFET equivalent circuit and short circuit current: Shows the MOSFET equivalent circuit and the process from when avalanche breakdown occurs until the short circuit current flows
Fig. 3 MOSFET equivalent circuit and short circuit current

The avalanche energy is given by:

The avalanche energy is given

EAS: Avalanche energy  IAS: Avalanche current  BVDSS: Drain-source breakdown voltage
VDD: Power supply voltage  tAS: Avalanche period   PA: Power during avalanche  L: Inductance

2. Current Destruction Caused by a Parasitic Transistor
When the drain-source voltage of a MOSFET exceeds its rated VDSS and avalanche breakdown occurs, avalanche current (IAS) flows into the internal resistance RBE, as shown in Fig. 3. This causes a voltage to develop across the base-emitter junction of the parasitic bipolar transistor (BJT), expressed as:
VBE=IAS×RBE ​
f this VBE becomes sufficiently large, the parasitic transistor turns on, allowing a large current (short-circuit current) to flow. This can lead to catastrophic failure of the MOSFET due to short-circuit destruction.

Countermeasures Against Avalanche Breakdown
To prevent MOSFET damage caused by avalanche breakdown, the following countermeasures are effective:

・Selecting Devices with Sufficient Margin:
Choose MOSFETs with a drain-source voltage rating (VDSS) that includes a sufficient margin above the maximum voltage expected to be applied.
Some products guarantee avalanche tolerance as part of their absolute maximum ratings, including allowable single-pulse current and energy. An example is shown below:

Table 1 Avalanche warranty (TK040N60Z1)
Item Symbol Rating Unit
Single-pulse avalanche energy     (Note) EAS

1049

mJ
Single-pulse avalanche current IAS 8.0 A

Note :VDD = 90V, Tch = 25℃ (initial), L = 29mH, IAS = 8.0A

・Minimizing Parasitic Inductance in Wiring:
Keep the wiring to the load (current-carrying paths) as short and thick as possible.
Using compact or surface-mount packages can also reduce lead inductance.

・Increasing Gate Resistor Value:
By increasing the gate resistance, the switching speed is reduced, which lowers the rate of change in drain current (di/dt).
The surge voltage VS​ is determined by the following formula:
  VS = LS * di/dt
Reducing di/dt helps suppress surge voltage.
However, slower switching increases the transition time from on to off, which can lead to higher switching losses. Therefore, select an optimal gate resistance value that balances surge suppression and power loss.

・Using Snubber or Clamp Circuits:
These circuits help suppress surge voltages that occur when the MOSFET switches from on to off. They absorb the energy stored in parasitic inductance, protecting the device from overvoltage stress.

Related Links

The following documents also contain related information.

Parametric Search

MOSFETs

FAQs

* Company names, product names, and service names used in this FAQ may be of their respective companies.

A new window will open