This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
The frequency bandwidth of transmittable digital signals depends on how LED current IF and load resistance are selected. It also depends on whether the current transfer ratio (CTR) is high or low. For transistor couplers, since the actual value for Propagation Delay Time is in the area of several tens of μs, the bandwidth is in the range of several kilobits to a dozen or so kilobits per second.
For details, refer to Toshiba Application Note "Basic Characteristics and Application Circuit Design of Transistor Couplers", section 2-4-3.Setting of Pull-up Resistance RC(max) and 2-4-4. Setting of Pull-up Resistance RC.
(https://toshiba.semicon-storage.com/ap-en/semiconductor/knowledge/application-note.html)