This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
When using a photocoupler with the base terminal (TLP731, for example), if the base terminal is left open, it works as an antenna and becomes likely to receive external noise easily. Especially, if a pulsed high voltage is applied between the input and output devices, induction noise received by the lead terminal of the base terminal and noise that flows by passing along the capacitance (input to output) are added, making the photocoupler operate as if there were input signals. In such a case, malfunction can be prevented by inserting capacitor CBE in the output transistor between the base and the emitter to absorb transient noise on the base terminal with CBE. However, this makes the output signal response rate slow. Care should be taken.