This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Video, audio and control signals are generally transmitted through an electric wire made of copper.
In contrast, a method for sending these signals as optical signals and converting them back into electric signals on the receiver side is generally called "optical transmission" or "optical communication."
The optical signals are transmitted through optical fiber. Conversion from electricity into light is called "E/O conversion," and conversion from light back into electricity is called "O/E conversion."