This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
In recent years, the size reduction in electronic equipment, high-density mounting, and severe operating conditions such as high ambient temperatures have caused a variety of heat issues when selecting, placing electronic components to be used and designing boards. Therefore, the importance of thermal design using cooling simulation with three forms of heat transfer: thermal conduction, thermal convection, and thermal radiation, is increasing.
Thermal models, such as the enclosure, the board, and the mounted components are required for cooling simulations. Toshiba Electronic Devices & Storage Corporation ("Toshiba") has created the Simplified CFD Model that is suitable for cooling simulations, focusing on MOSFET, and has started releasing this model. Simplified CFD Model can be used with thermal fluid analysis tool to visualize three-dimensional behavior (temperature distribution and flow velocity).
Please refer to the application note for the usage of the Simplified CFD Model.
Figure 2 shows a simulation result of which losses are applied to a MOSFET and heat is generated. It shows heat spread to the board and heatsink as MOSFET temperature rises.
Figure 3 shows the air velocity and heat flow in the chamber set during the analysis. The flow velocity and path of fluid (air) around the board can be checked.
Please refer to the following web page for the list of MOSFETs with Simplified CFD Model.
Thermal Management for Designs Using Discrete Semiconductor Devices
There are several effective ways to manage the high temperatures of today’s discrete semiconductors in your design.