This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
If I / O with different signal levels is connected, the driver’s output voltage level may not satisfy the input voltage specifications of receiver, resulting in malfunction or damage to the receiver. It is convenient to use a level shifter to solve such problems.
What kind of abnormality may occur if the voltages between the devices do not match? Here are two examples:
The first is when inputting a signal from a high voltage level to a low voltage level device, as shown in the upper right figure. Devices on the low voltage side often have a low withstand voltage of the input circuit, and if a voltage higher than the withstand voltage is input to it, it may be damaged and destroyed.
The second is when a signal is input from a low voltage level to a high voltage level device as shown in the lower left figure. If a voltage near the input threshold is applied to a device on the high voltage side, the high level signal cannot be recognized, resulting in a malfunction.
A level shifter is required to solve these problems.
Please refer to the FAQ “the application example (5V ⇔3.3V)”.
What options do I have to perform level shifting from 5 V to 3.3 V and vice versa?