This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
The overcurrent protection function prevents damage to the IC and load by suppressing power consumption in the event of an error. If the output current exceeds the limit current (ILIM) due to a load error or short circuit, the output voltage and output current also decrease, thereby limiting the power consumed by the ICs and the load.
Basic circuit
Limited current ILIM-external resistor RILIM
This overcurrent protection has the advantage of being adjustable with an external resistor.
The resistor surrounded by a red frame in the circuit diagram shown at left is an external resistor RILIM.
With this external resistor, the overcurrent limit can be set to 0.5A~5A for TCKE8 Series.
This overcurrent limit and external resistor RILIM are shown in the diagram at right and the equation below it.
As shown in this graph, the overcurrent limit is determined according to the resistance value.
It has the advantage of improving design flexibility because the overcurrent limit can be set arbitrarily simply by changing one external resistor.
(Be sure to check the resistance value with the actual machine when selecting the resistance value.)
●Comparison of eFuse IC performance with conventional fuses
|
eFuse IC |
Polyfuse |
Chip fuse |
|---|---|---|---|
Rated current |
3 A (setting) |
3 A (Rated) |
3.1 A (Rated) |
Overcurrent Protection operation |
|
|
|
Overcurrent Protective operation |
|
|
|
Even if you think that poly fuses and chip fuses can protect the circuits, there is a possibility that the circuits cannot actually be protected.
This diagram compares the overcurrent protection operation among between the eFuse IC and Poly fuse and chip fuse.
(For comparative purposes, eFuse IC overcurrent setting, poly fuse, and chip fuse ratings are unified around 3A.)
When the overcurrent of 5A was applied,
When an overcurrent of 10A was applied,