1-9. Overvoltage protection function (overvoltage clamp)

For TCKE8 Series, when the input voltage of the VIN pin of the eFuse IC exceeds the overvoltage clamp value (OVC), the output voltage VOUT is limited to the overvoltage clamp value (OVC) so that the overvoltage is not applied to the subsequent IC or circuits. 

There are two types of overvoltage protection functions:

  • a type that clamps the output voltage
  • a type that shuts off the output voltage.

Please check the data sheet for details as it depends on the product.

For TCKE8 series
For TCKE8 series
For TCKE712BNL
For TCKE712BNL

Basics of eFuse ICs

Basics of eFuse ICs
In this e-learning course, you will learn the basics of eFuse ICs, including their functions, advantages over conventional fuses, applications, overcurrent, short-circuit and overvoltage protection, and inrush-current control.
1-1. What is the semi-conductor fuse eFuse IC?
1-2. Advantages of Semiconductor-fuse eFuse IC (1)
1-3. Advantages of Semiconductor-fuse eFuse IC (2)
1-4. Advantages of Semiconductor-fuse eFuse IC (3)
1-5. Comparison of eFuse IC performance with conventional fuses
1-6. Examples of applications where semiconductor fuses (eFuse ICs) are used
1-7. Overcurrent protection function (OCP)
1-8. Short circuit protection function
1-10. Slew rate control (Suppressing rush current)

Related information

A new window will open