1-5. Comparison of eFuse IC performance with conventional fuses

Only the eFuse IC cuts off the current path at high speed and does not allow a large current to flow.

Results of short circuit protection operation

 

eFuse IC

(TCKE812NL)

Polyfuse

Chip fuse

Rated current

3 A (Setting)

3.1 A (Rated)

3 A (Rated)

Interruption time

2 μs

2.9 S

7 μs

Protective operation review

Results of short circuit protection operation

Results of short circuit protection operation

Results of short circuit protection operation

It was confirmed that a large current of 70A or more flowed momentarily in the poly fuse and chip fuse, and the chip fuse was broken.

The figure above shows the result of comparing the short circuit protection performance between the eFuse IC and the conventional fuse (poly fuse, chip fuse).

We were checking how long the output current  turned off when the output is short-circuited to GND.
(For comparison, the overcurrent settings of the eFuse IC, poly fuses, and chip fuse ratings were unified around 3A.)

As a result, the off time of the eFuse IC on the left side was about 2 μs, while that of the poly fuse in the middle figure was about 3 seconds, and that of the chip fuse in the right figure was about 7 μs.

The peak current was also suppressed to about 35A by the eFuse IC.
On the other hand, conventional fuses did not fit in the measurement range, and a large current of 70A or more flowed.

Basics of eFuse ICs

Basics of eFuse ICs
In this e-learning course, you will learn the basics of eFuse ICs, including their functions, advantages over conventional fuses, applications, overcurrent, short-circuit and overvoltage protection, and inrush-current control.
1-1. What is the semi-conductor fuse eFuse IC?
1-2. Advantages of Semiconductor-fuse eFuse IC (1)
1-3. Advantages of Semiconductor-fuse eFuse IC (2)
1-4. Advantages of Semiconductor-fuse eFuse IC (3)
1-6. Examples of applications where semiconductor fuses (eFuse ICs) are used
1-7. Overcurrent protection function (OCP)
1-8. Short circuit protection function
1-9. Overvoltage protection function (overvoltage clamp)
1-10. Slew rate control (Suppressing rush current)

Related information

A new window will open