This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
The differentiation between using eFuse IC (electronic fuse) and load switch IC is mainly determined by "purpose," "required protection functions," "cost," and "design complexity."
The load switch IC is mainly used for reducing system power consumption and setting power supply sequences. In contrast, the eFuse IC is mainly used in USB, HDMI® Interface, and servers or storage systems in data centers, where hot-plug/hot-swap operations are performed.
For example, hot swap refers to the insertion or removal of connectors or boards while the system is operating with power supplied. At this time, the board or system being replaced may be subjected to overvoltage or overcurrent.
The optimal protection IC to protect the system from such abnormal conditions is the eFuse IC.
[Differences between eFuse IC and load switch IC]
Please refer to the following pages and documents for product lineup and other documents.
* The terms HDMI, HDMI High-Definition Multimedia Interface, HDMI Trade dress and the HDMI Logos are trademarks or registered trademarks of HDMI Licensing Administrator, Inc.
* Company names, product names, and service names used in this FAQ may be of their respective companies.