This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
There are load switch ICs incorporating two switches. After the load switch IC “breaks” one switch, the break-before-make circuit keeps two switches off until it “makes” the other switch. This prevents two voltage domains from being short-circuited during the changeover between two switches.
Please also refer to the following documents for related explanations.
Application note
To product list of load switch ICs :
Main web page about load switch ICs
Other information