This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
The power dissipation of a general-purpose logic IC can be calculated by obtaining the static current and dynamic current, and then multiplying that current by the voltage applied to the IC.
Power dissipation can be obtained by multiplying the above current by the voltage applied to an IC.
Static power dissipation: PS
While general-purpose logic ICs are in a static state (i.e., while its input signal remains unchanged), little current flows in it except tiny leakage current that flows across the internal reverse-biased pn junction (known as static supply current, ICC). Static power dissipation is ICC multiplied by the supply voltage.
PS = VCC x ICC
VCC: Voltage applied to a logic IC
ICC: Static supply current shown in the datasheet
Dynamic power dissipation
Dynamic supply current is the current that flows in general-purpose logic while its input transitions between High and Low. This current flows during the charging and discharging of capacitance. It is necessary to consider both parasitic capacitance (internal equivalent capacitance) and load capacitance. Dynamic power dissipation is obtained by multiplying this current by the voltage applied to the P-channel or N-channel MOSFET. Here, for the sake of simplicity, the VCC value at which the maximum current flows is used for power calculation.
Dynamic power dissipation due to load capacitance (CL): PL
PL is dissipated when an external load is charged and discharged as shown by the Fig. 1.
The amount of charge (Q) stored on the load capacitance is calculated as follows:
QL = CL x VCC
CL: Load capacitance
Let the output signal frequency be fOUT (= 1/TOUT). Then, the average current (IL) is expressed as follows:
IL = QL / T = CL * VCC * fOUT
Hence, dynamic power dissipation (PL) is:
PL = VCC * IL = CL * VCC^2 * fOUT
If an IC has multiple outputs, its dynamic power dissipation can be calculated as follows:
PL = VCC^2 * Σ (CLn* fOUTn)
Dynamically Consumed Power with Equivalent Internal Capacitive CPD: PPD
General-purpose logic ICs have various parasitic capacitances as shown by Fig. 2. These capacitances are equivalently expressed as CPD. (Actually, CPD is calculated from power dissipation at relatively high frequency (1 MHz) under a zero-load condition.) PPD is the power dissipated by the equivalent capacitance of an IC and can be considered in the same manner as PL. Note, however, that PPD is calculated at input frequency (fIN):
PPD = VCC * IL = CPD * VCC^2 * fIN
Total Power Dissipation: PTTL
Total power dissipation (PTTL) can be obtained as the sum of static power dissipation (PS) and dynamic power dissipation (PL + PPD):
PTTL=PS + PL + PPD
The following documents also contain related information.