This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Answer
The TLCS-900 Family and TX19 Family offer products that contain the chip select/wait controller function. This function enables a chip select signal to be directly output from a microcontroller by setting data in the appropriate register.
TX03 Series have external bus interface that can be connected to SoC and external extended memory.
TX03 Microcntrollers having external bus interface:
(NO.EA9901901 2011/10/24)