This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Answer
AD conversion errors are measured in a unit called the LSB (least significant bit).
If the conversion error of an AD converter is specified as ±2 LSB, conversion results may include an error of ±2 digital values. For example, if an 8-bit AD converter has 0.0V to 5.0V conversion range and a conversion error of ±2 LSB, the AD conversion range of a 2.5V input, may vary in a range of 0x7e to 0x82. If the AD converter is error-free, the conversion result will be 0x80.
(NO.EA9901701 2011/11/01)