This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Gate-source zener diodes can be used to absorb surges within VGSS rating for short periods of time.
The gate-source Zener diode is designed to protect against ESD(Electro Static Discharge). It absorbs a large overvoltage (surge) within a short period of time and prevents a voltage above a certain voltage from being applied to other semiconductors.
The gate-source Zener diode is only for absorbing rare surges. Please confirm that an overvoltage larger than VGSS rating is not applied to the gate in the actual operating condition.
The drain-current (DC) that can be applied to a product is limited by the current carrying capacity of the product's package, the maximum-channel temperature and the safe operating area.
See also the pages and documentation below.