This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
When using a sensorless BLDC motor, caution is necessary for application with low speed rotation or significant load fluctuations.
Instead of using a sensor (Hall element or Hall IC) to detect the rotor position, sensorless drive monitors changes in motor induced voltage and predicts the motor energisation timing while driving.
However, the induced voltage is proportional to the rotational speed. As shown in Fig. 2, if the rotation speed of the motor is low, the induced voltage is also low. If the induced voltage is not sufficient, stable sensorless drive would be difficult and tends to result in unstable operation.
Also, sensorless drives also drive the motor by detecting changes in induced voltage while predicting the energisation timing. However, if the rotation speed of the motor changes significantly due to load fluctuations, the discrepancy between the required energisation timing and the predicted timing becomes large. As a result, the normally energised motor may be out of step(fail to rotate).
The following documents also contain related information.