This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
A current to be used should be at a level of current below the value specified with “ON-State Current ION” for the absolute maximum rating in the technical documents. In addition, since derating by temperature Ta is applied to ION, the level may become equal to or lower than the above value. Care should be taken. Even for a pulsed current and AC current, a current must be used with a value not exceeding the value for ION with respect to both the current peak value and the current effective value.