This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
The CR product is one of the important indicators for a photorelay to handle a high-frequency signal through the switch between the output terminals. "C" in this CR product refers to the output capacitance when the photorelay is OFF, COFF. "R" is the resistance between the output terminals when the photorelay is ON (ON-state resistance), RON.
When COFF is high, even if a photorelay is turned OFF, a high-frequency signal will pass through. If RON is high, loss when a signal passes through and deterioration will occur. Therefore, for applications that switch high-frequency signals, a photorelay with small COFF and small RON, i.e. a photorelay with low CR product, is required.