This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Optical fiber consists of a core that confines a light and a cladding that reflects it. Confined in the core, the light travels through it as it is reflected by the cladding.
Optical fiber composed of a plastic core and a plastic cladding is called plastic optical fiber (APF or POF). Optical fiber composed of a quartz glass core and a plastic cladding is called plastic clad quartz optical fiber (PCF), and the one composed of a quartz glass core and a quartz cladding is called quartz optical fiber.