This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Inrush current reduction is a function that suppresses the inrush current generated during switching with the slew rate control driver circuit (slow start circuit) built into the load switch IC. If the inrush current at each transient switching time increases significantly in the case where more than one power source is supplied from the PMIC, it may temporarily exceed the current capacity of the PMIC, causing a malfunction such as shutdown or system trouble. In order to prevent such a situation, it is necessary to suppress the inrush current.
We mass-produce load switch ICs with multiple slew rate control functions. If the output capacity is large, the inrush current (rush current) can be kept low by using the product with a slow slew rate (SRC3 in the figure above). On the other hand, if a fast VOUT start-up is required, the power supply can be controlled optimally by using products with a fast slew rate (SRC1 in the figure above).
Stock Check & Purchase
require 3 characters or more.