Comparison of eFuse IC performance with conventional fuses

Only the eFuse IC cuts off the current path at high speed and does not allow a large current to flow.

Results of short circuit protection operation

 

eFuse IC

(TCKE812NL)

Polyfuse

Chip fuse

Rated current

3 A (Setting)

3.1 A (Rated)

3 A (Rated)

Interruption time

2 μs

2.9 S

7 μs

Protective operation review

Results of short circuit protection operation

Results of short circuit protection operation

Results of short circuit protection operation

It was confirmed that a large current of 70A or more flowed momentarily in the poly fuse and chip fuse, and the chip fuse was broken.

The figure above shows the result of comparing the short circuit protection performance between the eFuse IC and the conventional fuse (poly fuse, chip fuse).

We were checking how long the output current  turned off when the output is short-circuited to GND.
(For comparison, the overcurrent settings of the eFuse IC, poly fuses, and chip fuse ratings were unified around 3A.)

As a result, the off time of the eFuse IC on the left side was about 2 μs, while that of the poly fuse in the middle figure was about 3 seconds, and that of the chip fuse in the right figure was about 7 μs.

The peak current was also suppressed to about 35A by the eFuse IC.
On the other hand, conventional fuses did not fit in the measurement range, and a large current of 70A or more flowed.

eFuse IC基礎知識

Basics of eFuse ICs
介紹eFuse IC的原理與優點、與傳統保險絲的比較、應用實例、過電流保護、短路保護、過電壓保護,以及以轉換速率控制抑制突入電流。
What is the semi-conductor fuse eFuse IC?
Advantages of Semiconductor-fuse eFuse IC (1)
Advantages of Semiconductor-fuse eFuse IC (2)
Advantages of Semiconductor-fuse eFuse IC (3)
Examples of applications where semiconductor fuses (eFuse ICs) are used
Overcurrent protection function (OCP)
Short circuit protection function
Overvoltage protection function (overvoltage clamp)
Slew rate control (Suppressing rush current)

Related information

開啟新視窗