This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
The Cross-Reference Multiple Parts Search is a convenient function available to logged-in members.
You can enter multiple part numbers from other manufacturers at the same time and display a list of Toshiba reference products in one search.
In the search box, choose Cross-Reference Search from the search options.
To use the Multiple Parts Search, please click “Search for multiple part numbers fromhere.”
* To use the multiple parts search function, Web membership registration is required.
Please proceed by clicking the New Member Registration button to register.
Enter multiple part numbers in the Cross-Reference Multiple Parts Search input box and perform the search.
The search results are displayed in a list format, showing the corresponding Toshiba reference parts.